Mouser Electronics Announces Global Distribution Agreement with murrplastik for Smart Cable Management Solutions
January 13, 2026 – Mouser Electronics, Inc., the authorized global distributor with the newest electronic components and industrial automation products, today announces a global distribution agreement with murrplastik, a leader in smart cable management systems and components for various industries and sectors worldwide. murrplastik's diverse portfolio includes products such as labeling systems, conduit and coupling systems, cable drag chains, cable entry systems, and dress packs for robotic applications. Additionally, they also manufacture products for the automotive industry and plastic products for the medical field.
This new agreement enhances Mouser's offering of reliable, high-performance cable management solutions that support modern industrial automation, machine building, robotics, and control panel applications.
The murrplastik Type KDL/E cable entry systems, now available from Mouser, feature an open-top, single-piece frame that enables quick insertion of pre-assembled cables. The snap-in design eliminates the need for screws, allowing fast and easy assembly. The KDL/E cable entry systems are suitable for standard cutouts for 16- and 24-pin industrial connectors and include a catch hook for 1.5mm to 2mm plate thickness. The systems are made of a polyamide 6.6 material, feature a UL 94V-0 flammability rating, and an IP54 protection rating when used with suitable grommets and cables.
The Type KDT/X cable entry grommets allow pre-assembled cables to be easily routed into and through control cabinets. The KDT/X series is designed for use with Murrplastik's KDL/C, KDL/D, and KDL/H cable entry systems, the KDT/X series is made from durable thermoplastic elastomer (TPE) and is UV-resistant, according to ISO 4892-2 standards.
The Type MSV conduit fittings are constructed with specially modified polyamide 6 that is free from halogen, phosphorus, and cadmium. These fully assembled fittings ensure that no parts are lost during shipping or installation. The murrplastik MSV conduit fittings comply with RoHS and ECE 324 R 118 standards and offer resistance to alcohol, grease, fuel, and mineral oil.
The Type KDL/D cable entry systems are offered in three variants. The KDL/D and KDL/D FDA versions are designed for standard cutouts for 6- to 24-pin industrial connectors and feature a 2-piece or 3-piece frame. The FDA compliant, ECOLAB approved KDL/D FDA version is ideal for use in food and pharmaceutical environments. The KDL/D-Mono series features a round, splitable construction for pre-assembled cables and standard M25, M32, M40, and M50 cutouts. All KDL/D cable entry systems provide an IP65 protection rating when used with suitable grommets and cables.
To learn more about murrplastik products available from Mouser, visit https://www.mouser.com/manufacturer/murrplastik/.
For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.
As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
2026 - murrplastik develops, produces, and distributes smart cable management systems and components for various industries and sectors worldwide. These cable management systems are designed for industrial machine automation, robotics, and maritime industries. Products include cable drag chain systems, flexible conduit and fitting systems, cable entry and holding systems, and wire marking, labeling, and engraving systems.
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.