Mouser Stocking New TE Connectivity / AMP's MCON 1.2 NextGen Sealed Locking Lance Connectors for Robust Automotive Applications

New Product Announcement

Connect With Us


Learn more about the MCON 1.2 NextGen connectors
Learn more about the MCON 1.2 NextGen connectors

May 6, 2026Mouser Electronics, Inc., the industry's leading New Product Introduction (NPI) distributor with the widest selection of semiconductors and electronic components™, is now shipping the MCON 1.2 NextGen sealed locking lance connectors from TE Connectivity / AMP Connectors. The MCON 1.2 NextGen connectors offer a sustainable, ultra-robust, and fully compatible alternative to the MCON standard and the Gen2 series. The MCON 1.2 NextGen connectors are designed for harsh automotive environments and are used in applications such as powertrains, safety and security systems, driver information systems, and body and chassis systems.

The TE Connectivity/AMP MCON 1.2 NextGen sealed locking lance connectors, now available from Mouser, also reduce carbon dioxide (CO2) emissions by up to 40% without sacrificing functionality. When using an optional biomass-balanced solution, the MCON 1.2 NextGen series further reduces the carbon footprint. The MCON 1.2 sealed locking lance connectors offer enhanced vibration performance (SG4) and an improved connector position assurance (CPA) design to ensure robust and secure connections in automotive applications.

The connectors also feature an integrated secondary lock latch with a large contact area for automatic locking. A 2-lip seal provides a tighter, more secure fit on the housing, and dress covers provide additional protection. The MCON 1.2 NextGen series is a highly versatile solution that uses the same interface across multiple applications in the vehicle and is fully compatible with standard MCON and the Gen2 Series. The MCON 1.2 NextGen connectors are available in two or three positions with a 1.2mm (0.047") mating tab width and a 4mm (0.157") centerline (pitch). The connectors are 48V-ready and ready for automation.

To learn more, visit https://www.mouser.com/new/te-connectivity/te-mcon-receptacle-housings/. For more Mouser news and our latest new product introductions, visit https://www.mouser.com/newsroom/.

 

As a global authorised distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed up the design process for customers, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Centre, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.

About Mouser

2026 - Mouser Electronics is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, mouser.com, is available in multiple languages and currencies and features more than 6.8 million products from over 1,200 manufacturer brands. Mouser offers 28 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 650,000 customers in 223 countries/territories from its 93,000m², state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.

About TE Connectivity

2026 - TE Connectivity is a global industrial technology leader creating a safer, sustainable, productive, and connected future. Our broad range of connectivity and sensor solutions, proven in the harshest environments, enable advancements in transportation, industrial applications, medical technology, energy, data communications, and the home. With more than 85,000 employees, including over 8,000 engineers, working alongside customers in approximately 140 countries, TE ensures that EVERY CONNECTION COUNTS. Learn more at www.te.com.

Trademarks

Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.

For further information, contact:
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
+1 (817) 804-3833
For press enquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
+1 (817) 804-7764