Mouser Press Room
Mouser Facebook Mouser Twitter Mouser RSS Feed Mouser YouTube Channel Mouser Google+ Mouser LinkedIn Mouser Subscription Center Mouser Blog
Mouser Press Room
New Product Announcement

 

Mouser Now Stocking ST's 6-Axis LSM6DS3 and LSM6DS33 Accelerometer/Gyroscope Modules

November 10, 2015 - Mouser Electronics, Inc. is now stocking the LSM6DS3 and LSM6DS33 3D accelerometer and 3D gyroscope modules from STMicroelectronics (ST). Part of the iNEMO® Ultra family of inertial MEMS sensor modules, the LSM6DS3 and LSM6DS33 deliver an optimized two-chip system-in-package (SiP) solution that combines always-on, low-power capabilities with ultra-low noise and superior sensing precision for mobile motion detection and analysis. These extremely compact 6-axis sensor modules boast industry-leading low-power performance down to 0.6 mA in always-on mode — a 20 percent improvement over other solutions.

The STMicroelectronics LSM6DS3 and LSM6DS33 3D accelerometer and 3D gyroscope modules, available from Mouser Electronics, have a full-scale acceleration range of ±2/±4/±8/±16 g, and an angular rate range of ±125/±245/±500/±1,000/±2,000 degrees per second, and offer industry-leading noise performance (90µg/√Hz and 7 mdps/√Hz, respectively). The modules operate from an analog supply voltage of 1.71 V to 3.6 V and are highly tolerant of mechanical shocks. Both modules offer I2C and SPI interfaces, and the LSM6DS3 module extends this communication through three different modes.

The modules' event-detection interrupts allow for recognition of free-fall events, 6-D orientation, tap/double-tap sensing, activity or inactivity, and wakeup events. The LSM6DS3 contains an on-chip sensor hub, which supports a total of six sensors: internal accelerometer and gyroscope, as well as support for up to four external sensors. The LSM6DS3 also supports the data acquisition of an external magnetometer with correction for hard- and soft-iron effects. An embedded temperature sensor in both modules also enables additional capabilities and broadens application possibilities.

The LSM6DS3 and LSM6DS33 modules are available through Mouser Electronics in ultra-small land grid-array (LGA) plastic packages that measure just 2.5 mm × 3 mm (LSM6DS3) and 3 mm × 3 mm (LSM6DS33). The modules are ideally suited toward a variety of low-powered, smart sensor applications such as handheld devices, wearable devices, indoor navigation, and innovative objects for the Internet of Things (IoT).

The LSM6DS3 and LSM6DS33 modules are supported by a full development platform, including the STEVAL-MKI160V1 adapter board, which is software- and hardware-compatible with the STM32 Nucleo Open Development Environment. The STEVAL-MKI160V1 adapter board can be plugged into the X-NUCLEO-IKS01A1 expansion board for STM32 Nucleo, enabling easy evaluation of the LSM6DS3 and LSM6DS33 modules in combination with other ST's MEMS and environmental sensors. The LSM6DS3 and LSM6DS33 modules are also supported by the STEVAL-MKI109V2 MEMS adapters motherboard, which provides a complete platform for evaluating ST MEMS products.

To learn more, visit http://www.mouser.com/new/stmicroelectronics/stm-lsm6ds3/.


With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 21 global support locations and the latest, most technologically advanced components for their newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.

About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 500 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 492,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.

Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.



Further information, contact:
Kevin Hess, Mouser Electronics
Vice President Technical Marketing
(817) 804-3833
Kevin.Hess@mouser.com
For press inquiries, contact:
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com
Back to Press Room