Now at Mouser: STMicroelectronics' VL53L0X Time-of-Flight Ranging Sensor Offers Fast Ranging of Greater Distances
August 1, 2016 - Mouser Electronics, Inc. is now stocking the VL53L0X laser-ranging sensor from STMicroelectronics (ST). The VL53L0X time-of-flight (ToF) sensor integrates a leading-edge single photon avalanche diode (SPAD) array and the second generation of ST's FlightSense™ technology to extend the measurement range up to two meters. The sensor offers ranging as fast as 20ms, and reports distance accurately regardless of target reflectance and color. The sensor supports a variety of applications, including user-detection in computers or tablets, landing assist for drones, and a wide array of functions in Internet-of-Things (IoT) devices.
ST's VL53L0X ToF sensor, available from Mouser Electronics, benefits from the same technology as ST's ToF sensor already being used in laser-assisted camera auto-focus in smartphones, and can distinguish movement towards or away from the sensor or from side to side. Distance is calculated internally and communicated over I2C, minimizing demands on the system host controller. The VL53L0X's integrated, eye-safe laser emits non-visible light of 940nm wavelength, which eliminates the distracting red glow typically associated with other infrared proximity sensors and improves immunity to interference from external light sources. Coupled with internal physical infrared filters, the laser enables longer distance ranging, higher immunity to ambient light, and better robustness to cover-glass optical cross-talk.
The highly energy-efficient sensor consumes only 20mW in active ranging mode and draws just 5µA in standby mode. At 2.4mm × 4.4mm × 1mm, it is the smallest ToF sensor on the market. The sensing capabilities of the VL53L0X can support a wide range of functions, including gesture sensing or proximity detection for user interfaces, obstacle detection for robotics, and hands-free operation of home appliances or industrial devices such as faucets and soap dispensers.
To learn more, visit http://www.mouser.com/new/stmicroelectronics/stm-vl53lox-sensor/
With its broad product line and unsurpassed customer service, Mouser caters to design engineers and buyers by delivering What's Next in advanced technologies. Mouser offers customers 22 global support locations and stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is updated daily and searches more than 10 million products to locate over 4 million orderable part numbers available for easy online purchase. Mouser.com also houses an industry-first interactive catalog, data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a subsidiary of TTI, Inc., is part of Warren Buffett's Berkshire Hathaway family of companies. Mouser is an award-winning authorized semiconductor and electronic component distributor, focused on the rapid introduction of new products and technologies to electronic design engineers and buyers. Mouser.com features more than 4 million products online from more than 600 manufacturers. Mouser publishes multiple catalogs per year providing designers with up-to-date data on the components now available for the next generation of electronic devices. Mouser ships globally to over 500,000 customers in 170 countries from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com